Enabling HTTPS connections for Enterprise Manager version 24.12. and higher 

This document assumes you have installed Enterprise Manager version 24.12 or higher and wish to enable SSL for HTTPS connections to the Enterprise Manager webpage. NOTE: For a trusted certificate, it is recommended that you purchase a third-party intermediate certificate from one of many online providers. Exacq cannot guarantee the legitimacy or security of a… Continue reading Enabling HTTPS connections for Enterprise Manager version 24.12. and higher 

Enterprise Manager memory resource usage high due to importer

Exacq Support has identified an issue with Enterprise Manager importer processes using an excessive amount of memory resource, often requiring reboot due to system becoming unresponsive when installed on some Windows machines. This is estimated to affect versions 23.06.2.0 thru latest versions of ExacqVision Enterprise Manager for Windows. Developers are aware and working on resolving… Continue reading Enterprise Manager memory resource usage high due to importer

SEQ – A guide to initial configuration for debugging Enterprise Manager Logs  

This guide will outline the steps needed to configure the tool SEQ on a PC in order to use scripts provided by Engineers at Exacq Technologies to aid in debugging Enterprise Manager Support Diagnostic Logs. Pre-Requisites: Initial installation and configuration steps in example – you could run the following commands:(use HTTP unless certs are configured)seqcli… Continue reading SEQ – A guide to initial configuration for debugging Enterprise Manager Logs  

Enterprise Manager Diagram

exacqVision Enterprise Manager (EM) provides a web-based dashboard to monitor system health, maximize surveillance uptime, manage large numbers of exacqVision system users, transfer camera licenses, and perform software updates across distributed exacqVision systems. Some level of enterprise management may be performed via the exacqVision Client for Enterprise licensed NVRs. But Enterprise licensing allows you to… Continue reading Enterprise Manager Diagram

Failing email notifications after update to Enterprise Manager version 23.09.9.0

April 4th, 2024 Enterprise Manager may fail to send email notifications after update to 23.09.9.0. ExacqVision support has identified an issue with failing email notifications after updating Enterprise Manager from a previous version to version 23.09.9.0 and up. This occurs when checking “Anonymous” as the send user, or additional configuration required for Exchange servers has… Continue reading Failing email notifications after update to Enterprise Manager version 23.09.9.0

Failover and Failback Issue in exacqVision Server and Enterprise Manager

Description  Level 3 Support has identified an issue with Failover functions in ExacqVision Server software manifesting as failback failure. The component responsible is ExacqVision Server software, but errors can be detected from the Enterprise Manager Failover Groups page as well, leading some customers to report this as an issue with the Enterprise Manager software. Product … Continue reading Failover and Failback Issue in exacqVision Server and Enterprise Manager

Can I Update My PostgreSQL Database?

Only the version of PostgreSQL installed by the Enterprise Manager installer is supported. <br> The exacqVision Enterprise Manager application provides a PostgreSQL installation to store Enterprise Manager data by default. The PostgreSQL Global Development Group may offer application updates that are not yet included within the ExacqVision Enterprise Manager installer. At times, users will seek… Continue reading Can I Update My PostgreSQL Database?

Can’t reinstall the EM server

When uninstalling Exacq EM server version 23.06 or above and reinstalling it again on the Windows unit, It will not complete the installation and ask to close the open session even if no sessions are open. Root cause The root cause of this issue is The Microsoft Open Database Connectivity (ODBC) that was not removed… Continue reading Can’t reinstall the EM server

Deploying System Lists to Client Users

In large organizations, such as multi-site enterprises, K-12 school districts, or university campuses, some admins will desire the ability to remotely manage the server connections their users have added within their ExacqVision Client application. This can result in faster deployments as well as less user support from their IT/Desktop Support teams, avoiding emailing, printing, or… Continue reading Deploying System Lists to Client Users

Outbound Connections tab in Client shows intermittent disconnecting then connecting

Some servers connecting to Integrator Services Portal or Enterprise Manager may show disconnected on outbound connections tab, then connected, and then disconnect again intermittently. Product  ExacqVision Server software ExacqVision Client software Steps to Reproduce  Expected Results  Status should remain “Connected” Actual Results  Status will show “Connected”, then momentarily show “disconnected”, then back to “Connected”, continuously… Continue reading Outbound Connections tab in Client shows intermittent disconnecting then connecting