Description On new installs of EM version 22.03.2.0 the passwords for emails settings to do not save to the DataBase. Product EM 22.03.2.0 Steps to Reproduce Install exacqVision Enterprise Manager version 22.03.2.0 Set up Emails settings and apply password in EM settings.Tested email with a IP camera disconnect.Logs Seen in the WebServer EM logs: Expected… Continue reading EM 22.03.2.0 issue with Passwords for Email Accounts not being saved in Data Base.
Tag: Enterprise Configuration
Configuring exacqVision S-Series Enterprise System with LSI RAID Controller with all JBOD Disks
exacqVision S-Series systems with LSI RAID controller running exacqVision Server 6.4.x display an empty Network tab on the Storage page if all disks are configured for JBOD. To fix this issue, complete the following steps: On the S-Series system, download the udev_gen.sh script (attached below).cd to the location where the script was downloaded and run sudo ./udev_gen.sh.… Continue reading Configuring exacqVision S-Series Enterprise System with LSI RAID Controller with all JBOD Disks