Description When installing the Pelco NET 6516 encoder and using Exacq server version 24.12, you may experience interruptions in the footage. Steps to Reproduce Install Pelco encoder NET 6516 with Exacq server 24.12.0 to 24.12.7 Expected Results You should see footage without any interruptions from the playback. Actual Results You will see interruptions in the… Continue reading The Pelco NET 6516 encoder experiences interruptions in the footage when used with Exacq Server version 24.12
Tag: Encoder
Motion Detection Fails on HikVision DS-6716HUHI-K Encoder
Description The HikVision DS-6716HUHI-K encoder fails to record when set to motion detection recording schedule in exacqVision. Note: This device has been deprecated by the manufacturer. Product Steps to Reproduce Expected Results Motion is detected and video is recorded Actual Results Motion is not detected and video is not recorded Solution We have found that… Continue reading Motion Detection Fails on HikVision DS-6716HUHI-K Encoder
Video Channel Fails to Connect With Error 551 on Samsung SPE-1610N Encoder
Description SPE-1610N encoders had video loss on the first channel of banks 2, 3, & 4. Also, the connection status would go from connected to Connection Error 551. Product exacqVision Server 19.12 Steps to Reproduce Add encoder as device type Samsung; add banks 2, 3, & 4 with the #bank=x override. Expected Results All channels… Continue reading Video Channel Fails to Connect With Error 551 on Samsung SPE-1610N Encoder
HD Analog Cameras are not Natively Supported on exacqVision Hybrid Servers
Title HD Analog Cameras are not Natively Supported on exacqVision Hybrid Servers Description exacqVision hybrid servers do not natively support HD analog cameras too include HD-TVI, HD-SDI, HD-CVI and AHD Product exacqVision Server Solution An encoder which supports HD analog will be required to connect an HD analog camera to an exacqVision… Continue reading HD Analog Cameras are not Natively Supported on exacqVision Hybrid Servers
Adding Multi-Channel Encoders
Description In order to accommodate more than 4 channels of video, many multi-channel encoders require the use of the “bank” IP plugin override. The cameras test records should indicate this in the Notes. Solution For Example, assuming the cameras IP address is 192.168.1.1: 1st bank would be:192.168.1.12nd bank would be:192.168.1.1#bank=23rd bank would be:192.168.1.1#bank=34th bank would be:192.168.1.1#bank=4… Continue reading Adding Multi-Channel Encoders
Axis encoders erroneously display video loss message
Affected Versions exacqVision Server 7.4 <br> Description Axis encoders display video loss message even when the video is being received and displayed. <br> Resolution Update exacqVision Server to version 7.8.0 or higher
E-Series 4-ch Encoder Fails to Record Secondary Streams for Inputs 2-4
Symptom: Secondary context streams may not record from scheduled or event linking recording. <br> Problem: Invalid generation of context elements in XML. <br> Solution: Upgrade exacqVision Server to version 9.7.13.99496 or higher. Optional Workaround: Add context streams with the RTSP plugin to record the secondary streams for inputs 2-4. rtsp://IPADDRESS/h.264/ch1/sub/av_stream#timestamp=rtcp
Tyco HD Encoder
E-Series 1-channel and 4-channel Official Firmware Version
INTERNAL NOTE: E-Series Encoders are EOM and non-NDAA compliant devices. <br> Some E-series encoders are having trouble with network communication. Attempts to connect with ExacqVision server, E-series utility or even find using ARP commands fail. <br> It was found that some encoders were shipped with firmware 1.2.0.150420 pre-installed. This firmware is for testing only. <br>… Continue reading E-Series 1-channel and 4-channel Official Firmware Version
Vivotek VS8801 Encoder Enabling 2nd NIC for exacqVision
Title Vivotek VS8801 Encoder Enabling 2nd NIC for exacqVision Description This encoder requires the use of two IP addresses to view all 8 channels of video. The first NIC allows access to channels 1-4 and the second NIC allows access to channels 5-8. The following are instructions for enabling the 2nd NIC on the Vivotek VS8801 encoder.… Continue reading Vivotek VS8801 Encoder Enabling 2nd NIC for exacqVision