Enabling Onboard Keyboard in exacqVision Ubuntu 10.04 and 12.04 Images

In 2013, the exacqVision Ubuntu 10.04 image was rebuilt, and the onboard keyboard configuration was not in included in the rebuild. Affected images can be easily identified by the Exacq wallpaper displayed on the Desktop. Also, because of an issue with onboard packages found in the Ubuntu repository, the onscreen keyboard was not included in… Continue reading Enabling Onboard Keyboard in exacqVision Ubuntu 10.04 and 12.04 Images