Description This article describes how to set IP addresses as either static or DHCP for a Cloudvue Gateways onboard NICs. Product Prerequisites Solutions NOTE: Network Settings can only be viewed, not changed from cloudvue.com Local Cloudvue Command Line In this example both NICs em2 (LAN) and em1 (Cameras) are being set to a static IP… Continue reading Configuring IP Addresses on a Cloudvue Gateway
Tag: Enabling DHCP
Enabling DHCP services on exacqVision recorders
Description Starting in exacqVision 7.4, the option to enable Dynamic Host Configuration Protocol (DHCP) services is provided. A DHCP server is used to provide IP addresses to any device on the network that requests address assignment.In exacqVision this feature can be used to more easily assign proper IP addresses to cameras. If multiple DHCP servers… Continue reading Enabling DHCP services on exacqVision recorders