Description The port drop down box will not allow you to change the port from SSL Port 465 to StartTLS Port 587. If selecting the StartTLS the port will not change to Port 587 which StartTLS uses. Product exacqVision Client 23.03.0.0 Steps to Reproduce When setting up an Email profile in the Email notification the… Continue reading Unable to Set StartTLS Email Notification Port