Affected platforms exacqVision 4.12.3 to 7.0 <br> Symptom There is a small memory leak whenever the server executes a program. This leak is unlikely to cause a problem on any desktop systems, but it could cause a hang or reboot on Edge systems with limited memory, if the Edge server is configured to send frequent… Continue reading Internal memory leak when sending email
Tag: Email
Server Email Notifications Broken
Symptom: Server fails to send email notifications. Problem: This issue was introduced with trunk 9.7.15, server will fail to send notification. Server logs may show the following: 10/8/2018 9:41:30 AM NotifyPI Error Failed to execute curl smtp operation using server gmail. (Profile Description: Gmail Profile) 10/8/2018 9:41:30 AM NotifyPI Error Failed to send notification using profile… Continue reading Server Email Notifications Broken
notifypi – failure to send email on falling edge
Description A NotifyPI enhancement was released with 8.4 which added the ability to specify ‘when’ to send an email: ‘Alarm Starts’, ‘Alarm Ends’ or ‘Alarm Starts and Ends’). However, the ‘Alarm Ends’ selection was failing to send the email when the trigger event (alarm) duration was shorter than the ‘Send Rate Limit’.If the event duration… Continue reading notifypi – failure to send email on falling edge