Description In some production environments, service accounts are used to run Enterprise Manager services. In order for the ElasticSearch to run it creates a tmp directory from the account it was installed under, this can cause the service to not run if you try starting the service as a different user. there are two ways… Continue reading Starting ElasticSearch service with a service account
Tag: ElasticSearch
Reverting to Apache Solr After Updating to ElasticSearch (Windows and LINUX)
IMPORTANT: It is advised to update to 22.3.0 so the customer have the capability of doing a backup, then proceed with the update to the version which uses elastic search. Prefix: It is not advised to revert back to a version using Apache Solr unless necessary. It is safer to do a fresh install if… Continue reading Reverting to Apache Solr After Updating to ElasticSearch (Windows and LINUX)