eDVR Video Playing Frames Out of Order Causing Stuttering

Issue: With live stream or playback video generated by the eDVR board set to MPEG4, the Client plays frames out of order resulting in stuttering video. Description: The video stutters — playing new frames, then older frames, creating a very jerky display effect. The video clip was MPEG4 with B frames. This seems to be… Continue reading eDVR Video Playing Frames Out of Order Causing Stuttering

Who manufactures Exacq video capture boards?

Exacq designs and manufactures its own video capture boards. Current tDVR capture board models are manufactured in Canada. Previous eDVR and sDVR capture boards, no longer manufactured, were designed by Exacq. Portions of the manufacturing process were performed by a contract manufacturer. <br>

Moving an eDVR Board in a Linux System

The following steps should be followed when moving the eDVR boards: In the exacqVision Client, save the system settings and note the serial number associated with the eDVR boards in the tree order by clicking on the board icons in the Configuration tree.Shut down the system.Unscrew the boards from the existing mounting. Do not disconnect… Continue reading Moving an eDVR Board in a Linux System