Setup and Licensing exacqVision Edge/Edge+

Description exacqVision Edge is a complete video management system (VMS) software solution that runs directly on an IP camera and stores video to an microSD/SD card inserted in the camera. Supported Devices Use the filters on the exacqVision IP Camera Integration database to search for devices that support exacqVision Edge. Installers Download the appropriate installer for… Continue reading Setup and Licensing exacqVision Edge/Edge+

Edge Server Application Stops Shortly After Starting on Illustra Cameras

Description Users setting up the ExacqVision Edge or Edge+ application on Illustra cameras may see the application running and connect to it only to find it stops running shortly thereafter. This is likely due to changing the default ‘Enable Event Record’ setting on the camera. <br> Product Cameras: Edge Server <br> Steps to Reproduce <br>… Continue reading Edge Server Application Stops Shortly After Starting on Illustra Cameras

Using exacqVision Web Service with Edge Cameras

Edge cameras cannot run the exacqVision Web Service. If you want to connect to an Edge camera using the Web Client or the Exacq Mobile 3 app you will need to install the exacqVision Web Service on another machine. The web service can be run on other machines but you will need to enter the… Continue reading Using exacqVision Web Service with Edge Cameras