Seen on Server 21.12If you have a customer having issues with not being able to record locally to the camera’s SD and not seeing the drive status in our client make sure to check the following in the cameras gui. Check the Configuration menu under Applications and Package Management to see if the “Save to… Continue reading Vivotek Edge not recording locally or displaying volume in the Exacq Client
Tag: Edge Cameras
Axis Edge losing config XML on power loss
In the ExacqVision Edge Server Trunk build version 21.06.114, We have improved our config persistence algorithm to guard against sudden power losses. you can download and use this version or wait until the next official release which is 21.09