E-Series encoders show invalid resolution and framerate after changing settings

Affected Versions exacqVision Server/Client 7.3.4 or later <br> Description After changing the framerate or resolution, exacqVision will show an invalid resolution and framerate <br> Workaround None <br> Resolution Update exacqVision Server and Client to 7.8.0 or higher <br>

Cannot connect more than 52 E-Series encoders to a server

Affected platforms exacqVision 4.10 to 7.0 (E-Series support introduced in 6.4) <br> Symptom When attempting to add the 53rd E-Series encoder to a server, the 53rd E-Series will not connect. On Linux platforms the server will crash. <br> Workaround If no Arecont, Illustra or UDP devices are being used on that server, install exacqVision development… Continue reading Cannot connect more than 52 E-Series encoders to a server