The DVI output on exacqVision systems with RAID controller cards might be deactivated on systems manufactured before 2011. This applied to all 4U and RAID exacqVision A-Series systems manufactured during that period. For those systems, you must use the VGA output when connecting a monitor.
Tag: DVI
VGA/DVI Monitor Adapter for First-generation iPad Not Compatible with exacqVision Client
The external VGA/DVI monitor adapter for a first-generation iPad is not compatible with Exacq Mobile 3. However, the adapter for iPad 2 is compatible with Exacq Mobile 3. <br>