Many users have moved to transporting files via portable USB devices or cloud services. CD/DVDs are still often desired by those working with legal evidence or those in insurance and law enforcement due to their low cost and ability to be mailed or stored in flat file folders. Users with systems that do not have… Continue reading CD/DVD Recorders and Disc Types
Tag: DVD
Using External USB DVD Drives with an exacqVision System
External USB DVD drives can be connected to an exacqVision system if they are compatible with the operating system (Windows 7 or Ubuntu 10.04 Linux). Although third-party USB DVD drives are not specifically supported or certified for use with exacqVision systems, Samsung SE-S084D/TSBS and LG GP08NU6B DVD drives have been successfully used for this purpose.… Continue reading Using External USB DVD Drives with an exacqVision System
Problems Exporting to CDs or DVDs
If you select files to export to a CD or DVD through the ExacqVision Client software, but you cannot actually burn the CD or DVD, it is possible that you are using low-quality optical disks. Try replacing the blank optical disk with a new one perhaps from a different manufacturer. Low-quality optical disks are prevalent;… Continue reading Problems Exporting to CDs or DVDs