PSMOVE For Windows

Description  The purpose of this KB is to help run PS MOVE and where to place the files on a system. Product  PSMOVE.exe Exacq Server 23.03 and above. File Location:  Windows:Place psmove.exe in the Server folder.Open powershell or command promt as ADMIN.cd C:\Program Files\exacqVision\Server and place the psmove.exe into the server folder. Linux: ETA not… Continue reading PSMOVE For Windows

Recording Not Possible – Windows DST Issue

Description  If the exacqVision Server data drives are full and are displaying “Recording Not Possible” on the storage page then it is possible an invalid hour folder was created during the switch to Daylight Savings Times (DST).  Use the following instructions to verify and resolve the issue.  Product  Solution These instruction are based on Windows… Continue reading Recording Not Possible – Windows DST Issue

Recording Not Possible – Linux DST Issue

Title Recording Not Possible – Linux DST Issue Description  If the exacqVision Server data drives are full and are displaying “Recording Not Possible” on the storage page then it is possible an invalid hour folder was created during the switch to Daylight Savings Times (DST).  Use the following instructions to verify and resolve the issue. … Continue reading Recording Not Possible – Linux DST Issue

Configuring DST/non-DST via client fails

Description Older servers/clients would allow you to configure the server’s timezone, but even though the DST radio button could be updated, it was in actuality treated as read-only, and would snap back depending upon the chosen timezone. As of server 8.1.3, the entire list of timezones has been completely revamped, the radio button removed, and… Continue reading Configuring DST/non-DST via client fails