EM failover is not moving the security integration list to the spare server.

Description  When the protected server goes down, and the EM server moves the configs to the Spare server, it will not move the Security integration list to the Spare server. Product  ExacqVision Server 32bit Steps to Reproduce  Installing ExacqVision 32bit version and trying to failover to it Solution Installing ExacqVision server 64bit version

Must use unique UDP port for each DSC Neo panel a server connects to

Affected platforms exacqVision 7.4 <br> Description When integrating to a Neo panel using UDP configuration, in the exacqVision Client a UDP port number must be specified. Using the panel’s default will work for the first panel configured for that server. For all subsequent panels, first change the application UDP port number in the panel to… Continue reading Must use unique UDP port for each DSC Neo panel a server connects to