Automation Control Circuitry

What is TTL? TTL stands for Transistor-to-Transistor Logic, where the “logic” determines which values are high and low. Standardized common TTL circuits operate with a 5-volt power supply. A TTL signal is defined as low when the voltage is measured between 0.0 V and 0.8 V with respect to the ground terminal, and high when… Continue reading Automation Control Circuitry