Description Drives showing offline or write error on Storage => Drive tab and Hardware tab. <br> Workaround Open Windows device manager (Windows start menu and type “device manager”)Expand IDE ATA/ATAPI controllersCheck to see if there are duplicate ATA Channel entries (ATA Channel 0, ATA Channel 1, etc)Disable the “Standard Dual Channel PCI IDE Controller” and… Continue reading Drives displaying “Red” on Storage Drive and Hardware tab