Downgrading ExacqVision Enterprise Manager from 23.06.0.0 to any version lower will prevent users from accessing the ExacqVision Client software due to the migration to AES-128 from ARC4 Encryption methods used on earlier ExacqVision Enterprise Manager versions. Downgrading or “Rolling Back” Enterprise Manager software from versions 23.06.0.0 and up to a lower version is not recommended… Continue reading Downgrading Enterprise Manager software from 23.06 to lower versions
Tag: Downgrading Enterprise Manager
Downgrading Enterprise Manager to 19.06 and below
Issue Downgrading exacqVision Enterprise Manager from 19.09 to any version lower will fail due to the migration from Python2 to Python3. Manual steps will be required in order to downgrade to 19.06. <br> Note: Instructions below provide a downgrade path to 19.06. If you need to downgrade beyond that, follow these instructions, then you can… Continue reading Downgrading Enterprise Manager to 19.06 and below