Issue If a Windows server is downgraded to a version before a new plugin was added, an upgrade back will not install those plugins by default; this means that an on-server upgrade is needed in order to select the checkboxes during install. Two notable plugins added in 19.09.0: ccurepi (used to connect to CCure 9000… Continue reading Windows installer may not reinstall new plugins after downgrade/upgrade