Enterprise Manager downgrade from 24.03 not supported

Description Beginning with Enterprise Manager version 24.03.0.0 (or 23.09.124), downgrading will fail due the update of an underlying resource. We now utilize Django v3.2.23, which necessitated a change to the database schema. This will cause downgrade database migrations to fail. Prior to upgrading from 23.09 or lower, it is recommended to complete a Backup. Instructions… Continue reading Enterprise Manager downgrade from 24.03 not supported

Downgrading Exacq software or camera firmware must be escalated

Downgrading Exacq software or camera firmware must be escalated Exacq Software Version If for any reason a customer must downgrade an exacq software version to resolve an issue, you must gather all applicable data (Support diagnostics, Wireshark capture) and escalate to L3 even if the issue has been resolved by downgrading. Downgrading the s/w version… Continue reading Downgrading Exacq software or camera firmware must be escalated

Downgrading exacqVision Web Server

Issue Due to the configuration migration which occurs when upgrading to exacqVision Web Server 9.6 you can not downgrade from 9.6 or higher versions to 9.4 or earlier versions using an older installer.  <br> To downgrade to a version of exacqVision Web Server prior to 9.6 you must completely uninstall exacqVision Web Server and then… Continue reading Downgrading exacqVision Web Server

Downgrading Software on Ubuntu/Linux OS

Ubuntu/Linux uses the ‘gdebi’ package installer to run .DEB packages. This will automatically check if you are attempting to install an older package than is already installed and warn you if a newer version is already installed. If you choose to downgrade the version of your ExacqVision Server, Client, or Web Service software you will… Continue reading Downgrading Software on Ubuntu/Linux OS

Do not downgrade Illustra camera firmware on cameras that use iAPI3 interface

Affected Platforms Illustra cameras running firmware that supports the iAPI3 inteface, including the i625 PTZ, i825 Fisheye and 2/3/5 MP Pro series models. Description Do not downgrade the firmware on any Illustra cameras using the iAPI3 interface. This can cause corruption and some iAPI3 requests could return “Internal Server Error” messages. In some cases, video… Continue reading Do not downgrade Illustra camera firmware on cameras that use iAPI3 interface