Description
Beginning with Enterprise Manager version 24.03.0.0 (or 23.09.124), downgrading will fail due the update of an underlying resource. We now utilize Django v3.2.23, which necessitated a change to the database schema. This will cause downgrade database migrations to fail.
Prior to upgrading from 23.09 or lower, it is recommended to complete a Backup. Instructions for scheduling a backup can be found in the exacqVision Enterprise Manager User Manual HERE.
NOTE: If you are using Postgres DB, you will only need the backup file. If using MS SQL, you will also need to create a DB backup utilizing Microsoft utilities. More information can be found HERE.