Description
If using esm api docs at /docs/api, any file upload/download action will not work.
The documentation does not even provide the correct input to upload/download files.
<br>
Version Introduced
v3.8.0.89234
<br>
Platform
All.
<br>
Steps to reproduce
- Navigate to http://esmhost/docs/api, once fully loaded,
- Click on system
- Click on [GET] /api/system/logs/bundle/
- Click on [Try it out!]
<br>
Expected result
- File is downloaded during file download
- Upload button/handle is provided to upload file
<br>
Actual result
- Documentation page will just try to display the contents of the file on download.
- There is no upload button/handler
<br>
Work around
- Get logs using browser at http://esmhost/api/system/logs/bundle, OR use command line tools to get logs from http://esmhost/api/system/logs/bundle
- This is the same for any other file upload or download
<br>
Version fixed
19.09.0
<br>
ESM-API-api-docs-does-not-support-file-upload-download.pdf