Secondary DNS Entry Clears Network Settings in 12.04

Problem: Server version 9.2.1 added the ability to set a secondary DNS address to the network interface settings. This is broken when using on Ubuntu 12.04.  <br> Symptoms: When applying a secondary DNS address, all settings change to 0.0.0.0 and/or the NIC fails to apply any changes.  <br> Solution: Update Server to 9.2.3