Description Refer to #d17458. Apparently, DMP intrusion panel model XR550 requires the remote key to be 8 characters long, all capitalized. If your remote key is less than 8 characters, you need to enter trailing spaces into exacqVision to get 8 characters. If your remote key contains any lower-case characters, you need to enter capitals into… Continue reading DMP intrusion panel XR550 requires 8 characters and all capitalized
Tag: DMP
DmpPi Slow To Reconnect
Issue The DMP panel uses a ‘disconnect’ command to gracefully close a socket. The original release of the DmpPI plugin did not implement this command. As a result, after a connection to a panel was made, then was disabled and quickly enabled again, the connection attempt failed several times until the panel timed out and… Continue reading DmpPi Slow To Reconnect