Description
Illustra Flex4 Indoor PTZ with bubble showing distorated images on zoom.
Product
Illustra Flex 4 PTZ all firmware
Steps to Reproduce
Turn off the Tilt Limit in the camera PTZ settings
Expected Results
Camera zoom shows in focus and sharp
Actual Results
Camera zoom is slightly disorted and out of focus
Solution
This is working as designed.
The camera datasheet indicate the tilt range is -15 to -90.
When you disable the tilt limit and move above -15 degree, you will see image distortion at zoon due to the camera looking through the ‘transition region’ of the bubble.