Nested in the configuration tree, beneath Camera Recording, is the list of all cameras connected to the system. Clicking on any of these cameras will display the settings page for that individual camera. From here, you have access to important settings, such as the camera name, configuring the optional on-screen display (OSD), picture settings, motion… Continue reading Camera Settings
Tag: Display
System will not post without monitor attached
These files are only to be ran on ExacqVision Servers with the following Motherboards. DO NOT try to run it on your machine or it will cause issues!!! With the rise of new HIPPA requirements regarding patient information potentially being exposed on systems, a lot of customers are choosing to run their NVR’s Headless (no… Continue reading System will not post without monitor attached
On-screen Time Display is Incorrect and Recorded Video Cannot be Found
Background Information Diagnostic Steps Resolution <br>
Does the ExacqVision Client Support Multiple Monitors?
Yes, ExacqVision Client supports multiple monitors. We have tested up to four VGA monitors from a single workstation. Typically, a user will run one instance of the ExacqVision Client per monitor. Because decompressing video is CPU-intensive, we recommend one core per Client for the best user experience. To drive up to four VGA monitors, we… Continue reading Does the ExacqVision Client Support Multiple Monitors?