Cloudvue Manager C2C Disk Space

Description The disk space section in Cloudvue Manager for C2C devices returns a listing of the partitions on the camera and the microSD card.It is equivalent to running the Linux command df -h SD Card Status Green – Healthy Ideally the SD card will show a status of green with a message of SD Card… Continue reading Cloudvue Manager C2C Disk Space

Troubleshooting 100% Smartvue Partition Disk Space Usage

Description  The Disk Space Use% for the partition mounted as /smartvue should not reach 100%.  If it does odd behavior too include loss of live or recorded video may occur.  Further troubleshooting should help decide if the issue is related to a failed or failing hard drive or a corrupted database. Product  Steps to Reproduce … Continue reading Troubleshooting 100% Smartvue Partition Disk Space Usage

Corrupted cloud-config.json File 

Title Corrupted cloud-config.json File  Description  Customer reported that they could no longer view live video in Cloudvue Web or Cloudvue Mobile App.  Additionally, Disk Space would not load. Product  Solution We were able to use the failover port to gain SSH access to the Cloudvue Gateway and replace the corrupted configuration file /smartvue/cloud-config.json