One way to determine if the drive is failing in Linux is to run the following command in the terminal dmesg | lessĀ This should give you an error list you can scroll through for read/write errors. If you see a problem on a data drive perform the following: If the problem shows on the… Continue reading How to force disk check (fsck) in Linux.