IPCamDetect crashes on Una server when camera disconnected from port during discovery/addressing

Affected platforms exacqVision Server 7.4 on Una LC servers <br> Description When a discovery scan and auto-addressing is interrupted by unplugging a camera from the Una POE ports or the port is power cycled, IPCamDetect could crash. This can happen when a camera is connected to one of the UNA ports, which triggers an auto… Continue reading IPCamDetect crashes on Una server when camera disconnected from port during discovery/addressing