Description The Cloudvue Gateway video file storage structure is as follows: Product Solution /smartvue/video/MAC/YYYY-MM-DD/EPOCHTIME.mp4 MAC (The MAC address of a connected camera)YYYY (Year such as 2023)MM (Month such as 03 for March)DD (Date such as 30 for the 30th)Note: The folders Year, Month Date are UTC/GMT not the local time zone of the Cloudvue Gateway.… Continue reading Cloudvue Gateway – Video File Naming Format
Tag: Directory Structure
exacqVision Video File Naming Format
2040–00160380.ps min/sec manufacturer device id storage rule <br> exacqVision files are stored on each drive enabled for recording in a directory structure as follows: <br> Within each directory, video is stored in files with duration of five minutes. Each device (IP camera, compression board, encoder) has its own files. The file naming convention is as follows: MMSS-XXXXYYZZ.ps and MMSS-XXXXYYZZ.psi.… Continue reading exacqVision Video File Naming Format