Jagged Edges Appear on Sony SNC-HM662 Using Third Party Dewarper

Description  When using the Immervision dewarper on the Sony SNC-HM662 jagged edges will appear in the live view of the camera. Product  Any ExacqVision NVR Steps to Reproduce  Expected Results  You are able to utilize DPTZ with no issues Actual Results  Jagged edges appear around the camera’s view Solution The issue resides on the third… Continue reading Jagged Edges Appear on Sony SNC-HM662 Using Third Party Dewarper

Camera Settings

Nested in the configuration tree, beneath Camera Recording, is the list of all cameras connected to the system. Clicking on any of these cameras will display the settings page for that individual camera. From here, you have access to important settings, such as the camera name, configuring the optional on-screen display (OSD), picture settings, motion… Continue reading Camera Settings

Saved Digital PTZ View displays incorrectly when searching

Product exacqVision Client 6.0 to current <br> Description If you use the same video input, one with digital PTZ enable and zoomed in and the other with Digital PTZ disabled, the saved view will not display as intended when searching that view on the Search Cameras page. <br> Solution Enable Digital PTZ on both instances.… Continue reading Saved Digital PTZ View displays incorrectly when searching