Description As a result of KB https://support.exacq.com/#/knowledge-base/article/5610 the C1410 MK II can not alone create event linking to trigger through Exacq software. Exacq currently does not support the use of webhooks seen in the above KB. This guide will assist you with configuring an Axis D3110 Connectivity Hub to trigger the C1410 MK II via… Continue reading Using an Axis D3110 Connectivity Hub with the Axis C1410 MK11 Speaker
Tag: Digital Output
Using Axis Networked Speakers with exacqVision for Pre-Recorded Clips
Description Axis networked speaker(s) are individually capable of having pre-recorded audio clips loaded onto them for playback. Audio effects such as door bells, barking dogs, event announcements, and more may be desired for a given site. Models C1410 / C2005 Playback of audio files from the network speaker(s) cannot be triggered through exacqVision Client or… Continue reading Using Axis Networked Speakers with exacqVision for Pre-Recorded Clips
Axis plugin with newer fw failed to trigger digital output
Description This affects Axis cameras with firmware 5.70 and above, that started using Apache HTTP server. Apache HTTP server is more restrictive in parsing non URI characters such as simicolon and slash and requires percent encoding. For example, “:/” would be encoded into %3a%2f. The end result is that it affect the triggering of digital… Continue reading Axis plugin with newer fw failed to trigger digital output