Symptom: On a Linux system configured for DHCP the exacqVision Client network settings page displays 0.0.0.0 as the primary DNS. <br> Problem: This is may be cosmetic, the actual primary DNS for the server should be correct IF a primary DNS is assigned from the DHCP server. <br> Solution: Update the exacqVision Server to version… Continue reading Primary DNS Shown as 0.0.0.0 on Linux Server Configured for DHCP
Tag: DHCP
Enabling DHCP services on exacqVision recorders
Description Starting in exacqVision 7.4, the option to enable Dynamic Host Configuration Protocol (DHCP) services is provided. A DHCP server is used to provide IP addresses to any device on the network that requests address assignment.In exacqVision this feature can be used to more easily assign proper IP addresses to cameras. If multiple DHCP servers… Continue reading Enabling DHCP services on exacqVision recorders