Legacy Arecont Camera Frame Rates

Description  Arecont Legacy cameras are limited to the amount of Frames Per Second they send when using Full Resolution vs Half Resolution.Example of Cameras:Arecont AV12176DN-NLArecont AV2455DN-FArecont AV5555DN-S Product  If you find that the Received Frames Per Second or Decoded Frames Per Second are Half the FPS it is due to the limitations of the cameras… Continue reading Legacy Arecont Camera Frame Rates

Lower Frame Rates Displayed than Expected

At times, the number of frames per second displayed on an exacqVision system might be lower than expected. This can be caused by network bandwidth, the processor, or the display driver. To determine the cause of the issue, click the kB/s indicator in the exacqVision Client status bar multiple times to cycle through the following… Continue reading Lower Frame Rates Displayed than Expected