Affected Versions <br> Description In web service 7.6 (Windows only), dewarping of Dahua fisheye cameras does not work. These cameras do not show any dewarping options in the web client or Exacq Mobile 3 app. <br> Workaround <br> Resolution Update exacqVision Web Service to version 8.2.2 or higher <br>
Tag: Dewarping
Axis fisheye camera dewarping and the exacqVision Web Service
Only supported on Ubuntu 12.04, Ubuntu 14.04, Windows 7, 8, and Windows Server 2010.These instructions are dependent upon your system supporting OpenGL 3.0 or higher. WINDOWS On an exacqVision Server, change the Operating System to automatically login to “admin” following the instructions in KB 45061.Place the attached webservice_fisheye_fix.bat file into your auto-login user’s Desktop.Use the Windows Task Scheduler… Continue reading Axis fisheye camera dewarping and the exacqVision Web Service