The Device Type I need isn’t listed

Details When adding an IP device to your ExacqVision Server, each device will be associated with a Device Type that selects the underlying plugin used for communication. The article, What IP cameras are supported by ExacqVision?, will tell you more about how to use the IP Camera Integration database to find the proper Device Type.<br><br>… Continue reading The Device Type I need isn’t listed

RTSP Plug-in used with ExacqVision Software

The RTSP plug-in supports generic streaming of audio and video using the RTSP/RTCP/RTP protocol. The plug-in automatically configures the streaming transport to either UDP or TCP. The default when the device is connected is TCP; if it fails to connect, it tries to connect through UDP. The plug-in does not support any configuration — it… Continue reading RTSP Plug-in used with ExacqVision Software