Axis with VMD4 reporting “Device reporting an error” and stream video

Description This is limited to Axis cameras supporting VMD4 (fw 6.50 and later) either after factory default or out of box. In this case, the plugin detects VMD4 is preferred over VMD1 and by default VMD4 is stopped. The Axis plugin in this case sends a request to start VMD4 and some camera model and… Continue reading Axis with VMD4 reporting “Device reporting an error” and stream video

Axis Displays “Device Reporting an Error”

Problem: An Axis camera may display the error “Device reporting an error, the device reported that is has encountered an error (500)” but continues to display a normal video stream.  <br> Explanation:  This is typically caused by a camera that does not have native PTZ functions but could be connected to an external PTZ device… Continue reading Axis Displays “Device Reporting an Error”