NOTE: It is recommended that you do NOT install this software on Windows XP Professional. <br> You can download Intel Desktop Utilities from the following location: http://downloadcenter.intel.com/Detail_Desc.aspx?agr=Y&DwnldID=18934&ProdId=3121〈=eng <br> If you are not using the server and need to manually download the drivers, complete the following steps: <br> Select Desktop Boards under Products.Select Intel® 4 Series Chipset… Continue reading Intel Desktop Utilities for Windows 7