In large organizations, such as multi-site enterprises, K-12 school districts, or university campuses, some admins will desire the ability to remotely manage the server connections their users have added within their ExacqVision Client application. This can result in faster deployments as well as less user support from their IT/Desktop Support teams, avoiding emailing, printing, or… Continue reading Deploying System Lists to Client Users
Tag: Deploying Client Settings
Deploying Client Settings for 9.2 and Earlier
When deploying exacqVision Client installations there are no client settings deployed with the act of installation. In certain network environments it is desirable for system or network admins to wish to deploy settings such as the server addresses and login credentials to Client users. While settings such as this aren’t included with the installation it… Continue reading Deploying Client Settings for 9.2 and Earlier