Description Level 3 Support has identified an issue with Failover functions in ExacqVision Server software manifesting as failback failure. The component responsible is ExacqVision Server software, but errors can be detected from the Enterprise Manager Failover Groups page as well, leading some customers to report this as an issue with the Enterprise Manager software. Product … Continue reading Failover and Failback Issue in exacqVision Server and Enterprise Manager
Tag: Data Restore Pending
Stuck Pinned Spare/Data Restore Pending due to firewall blocking vfba process
Exacq Support has identified an issue preventing fail-back due to VFBA.exe being blocked; which uses port 28774. Windows Versions It is recommended to create both inbound and outbound Windows firewall rules on the SPARE and PROTECTED server to allow communications through port 28774 for the Windows Firewall. ** Due to issues with the Window OS,… Continue reading Stuck Pinned Spare/Data Restore Pending due to firewall blocking vfba process