Dewarping of Dahua cameras not working on web client or Exacq Mobile 3 (Legacy)

Affected Versions <br> Description In web service 7.6 (Windows only), dewarping of Dahua fisheye cameras does not work. These cameras do not show any dewarping options in the web client or Exacq Mobile 3 app. <br> Workaround <br> Resolution Update exacqVision Web Service to version 8.2.2 or higher <br>

HTTPS for Illustra Essentials / Dahua cameras

To set the HTTPS mode for Illustra Essentials and any Dahua OEM cameras: Go to camera web pageEnable the HTTPS option in the Network/Connection section The camera will auto generate a self-signed certificate so that exacqVision may connect with HTTPS. Note that if the camera is in HTTPS mode and the camera’s IP address is changed,… Continue reading HTTPS for Illustra Essentials / Dahua cameras