Dahua/Illustra Essentials plugin failed to post NTP server address on the camera at startup.

Description Dahua plugin which also supports Illustra Essentials failed to set the NTP server on the camera during initial connection time. By default if there is no override ntp server, the plugin should push the address of the server as NTP on the camera. <br> Version Introduced r71495 (dev build 6.5.38.71503/RC build 6.6.0.71575) <br> Platform All… Continue reading Dahua/Illustra Essentials plugin failed to post NTP server address on the camera at startup.

IP Plugin Overrides

The standard form for exacqVision camera addresses is as follows: {host}{?parameter_1=value_1}…{?parameter_n=value_n}{#override_1=value_1}…{#override_n=value_n} <br><br> Overrides PluginOptionUsageACTitransport=httpHTTP stream support for legacy platforms and user dataACTitransport=rtspRTSP stream with separate metadata socket for motion/input trigger/video loss/etc.Axiszoom=configBy default zoom only cameras support.Axiszoom=operationForce zoom only operation and controls as part of PTZ and live view.Axisblocksize=offOn by default, but could turn off blocksize… Continue reading IP Plugin Overrides