The parameters of secondary streams (multistreams) that can be created in exacqVision are defined by the stream profiles defined in Samsung cameras. Samsung cameras ship with default profiles like H.264, MJPEG or mobile. These profiles each define a codec, default resolution and default framerate. For example the default camera profiles may not provide a second… Continue reading Create custom multistreams using profiles for Samsung cameras
Tag: Create Custom Multistreams
exacqVision Multistreaming on Illustra 825 Fisheye Cameras
If you want Stream 1 on an Illustra 825 Fisheye camera to be anything other than Fisheye, you must change it in the camera’s web browser. If you have aready configured multistreaming on the camera in exacqVision Client, you must delete the multistreams before changing Stream 1 in the browser.<br> The following stream combinations are… Continue reading exacqVision Multistreaming on Illustra 825 Fisheye Cameras