Pelco plugin with Optera crashes server

Description Pelco plugin with Optera crashes server. ExacqRtsp_lib getSdpValue function is used by Pelco Optera to get the dewarp information with the RTSP session. The camera fails to return sdp and the default return of the getSdpValue method is NULL in this case. Line 1148 ExacqRTSPCommandHandler.cpp. <br> Tested Version <br> Steps to reproduce <br> Expected result Server… Continue reading Pelco plugin with Optera crashes server