Affected platforms
exacqVision Server 7.4 on Una LC servers
<br>
Description
When a discovery scan and auto-addressing is interrupted by unplugging a camera from the Una POE ports or the port is power cycled, IPCamDetect could crash. This can happen when a camera is connected to one of the UNA ports, which triggers an auto scan on the port. Then during the auto-addressing, the camera is unplugged.
<br>
Workaround
None
<br>
Resolution
Update exacqVision Server to version 7.6.2.94278 or higher