Description Server crashes when add Axis camera with date/time on the camera is set to sync manually or with computer time. <br> Version introduced 8.6.1.115070 <br> Platforms All <br> Steps to reproduce In the camera web page, change the “Time mode” to either manual or with computer time in “Date & Time Settings” page.connect Axis… Continue reading Axis crash server with date/time settings