Cameras Added With the Wrong Plugin Causes exacqVision Server Crash Loop

Description Adding certain cameras with the wrong plugin type causes the exacqVision Server to go into a crash loop. Product Steps to Reproduce Expected Results Actual Results Solution NOTE:  This has been specifically observed when Illustra cameras are added with Illustraflex instead of Illustra3 and Samsung cameras are added with Onvif instead of Samsung <br>

Server Fails to Fully Restart After Crash if there is No Watchdog

Symptom: The sever fails to fully restart after a crash.  <br> Problem: If the server crashes, exacqd will restart the server, but then exacqd exits. This causes the server to hang during initialization. If there is no watchdog timer, the server will remain in this state. The ‘core’ process should be killed. Introduced in server… Continue reading Server Fails to Fully Restart After Crash if there is No Watchdog