Warning: Level 2 Document – Please do not distribute. Introduction By default, the number of sub-importer processes spawned by Enterprise Manager will be equal to the number of logical CPUs. If that is not desired, the number can be controlled by setting the ‘_EM_NUM_IMPORTERS’ environment variable. On Windows this should be a system environment… Continue reading Importer Environment Variable – Overriding Default Values for Linux Enterprise Manager Servers
Tag: CPU Usage
High CPU Usage After Installing ESM 5.4.0
Problem: Users find high CPU usage with PostgreSQL or user databases after upgrading ESM to 5.4.0. <br> Solution: Fixed in ESM version 5.5.5
High CPU Usage Seen From ESM 5.8
Symptom: High CPU utilization is seen on system running ESM 5.8. <br> Problem: Over 100+ banner messages from ESM causes high CPU usage. CPU spikes every 15 seconds. <br> Solution: Update ESM to version 5.9.8 or later.