Registering Kantech EntraPass Corporate Edition requires a Kantech certified dealer to obtain a registration confirmation code from Kantech technical support or from the Kantech website registration. To setup the Kantech EntraPass Corporate Edition software, view the complete installation guide or watch this short video to walk you through the installation process. The installation allows you to setup basic system components… Continue reading How do I register Onboard Kantech EntraPass Corporate Edition on an ExacqVision recorder?
Tag: Corporate Edition
Can I upgrade Onboard Kantech EntraPass Corporate Edition on an exacqVision recorder?
Upgrading Kantech EntraPass Corporate Edition requires a Kantech certified dealer to obtain a registration confirmation code from Kantech technical support or from the Kantech website registration. For more information on the upgrade procedure to Kantech EntraPass Global Edition, please refer to the Kantech Reference Manual, DN1415-1310 page 20. <br>
Can I install Onboard Kantech EntraPass Corporate Edition on an ExacqVision recorder I’ve already purchased?
No, Kantech EntraPass cannot be installed on recorders that were purchased prior to February 9, 2016 without the CSA option. If a server was previously ordered with the CSA upgrade, you can obtain the installation and registration code from Kantech technical support or from the Kantech website registration. You may also view the FAQ page on the ExacqVision… Continue reading Can I install Onboard Kantech EntraPass Corporate Edition on an ExacqVision recorder I’ve already purchased?